Maximum permissible axial load for Cylindrical Roller Bearings
For Cylindrical roller bearings to have a stable axial-load carrying capacity,
○When axial loads are applied, radial loads must also be applied
(Axial load should be under approximately 40% of Radial load.)
○Sufficient lubricant must exist between the roller end faces and ribs.
○Superior extreme-pressure grease must be used.
○Sufficient running-in should be done.
○The mounting accuracy must be good.
○The radial clearance should not be more than necessary.
In cases where the bearing speed is extremely slow, the speed exceeds the limiting speed by more than 50%, or the bore diameter is more than 200mm,
careful study is necessary for each case regarding lubrication, cooling, etc.
In such a case, please consult with NSK.